CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimProjectUser Json Schema
CimProjectUser Json Schema
Description
Fields that need to be specfied for creating a user before enabling rest configuration for project
Overview
CimProjectUser
Fields that need to be specfied for creating a user before enabling rest configuration for project
ProjectID : string
The Id or name of the project.
ProjectPath : string
full absolute path to project specified in ProjectID
User : CimUser
Fields that describe the user
AuthenticationType : CimUserType
Enable : boolean
set it to true to enable the user.
PasswordExpiresInDays : number
password expires in number of configured days.
Password : string
Password for the user.
Resources : Array[string]
An array of resources that mapped to the user.
RoleID : string
The Id of role.
UserID : string
The Id of user.
UserName : string
The name of user.
Properties
NameDescriptionData Type
The Id or name of the project.string
full absolute path to project specified in ProjectIDstring
Fields that describe the userCimUser
 CimUserType
set it to true to enable the user.boolean
password expires in number of configured days.number
Password for the user.string
An array of resources that mapped to the user.Array[string]
The Id of role.string
The Id of user.string
The name of user.string
See Also